Read Time: 4 Min
The development of smarter aerospace and defense systems in 2026 and beyond will rely primarily on two sources: the immense processing power required for AI and the industry-wide goal of electrification. Advancing these digital capabilities, however, creates a direct conflict with the uncompromising demands of the physical world. Greater computational power generates more heat that must be managed within shrinking footprints, while geopolitical dynamics and soaring global demand strain supply chain stability. Embedding digital innovation into rugged, field-ready systems has become the defining engineering challenge for the industry, one that begins by understanding the key trends of electrification and AI.
Defining the Key Digital Trends: Electrification and AI
Electrification is a critical long-term opportunity for the aerospace and defense industry. The scope of this shift is significant, with applications extending from electric vertical takeoff and landing (eVTOL) aircraft and drones to electrification of land vehicles. The move toward electrification enables the adaptation and ruggedization of mature technologies from the commercial electric vehicle market. By building upon proven solutions, engineers can accelerate development cycles for aerospace and defense-specific applications, creating a critical advantage in this rapidly advancing field.
In contrast to the long-term horizon of electrification, AI is already producing immediate and tangible efficiencies in operational areas. AI is actively applied to optimize a range of activities, from sourcing and production floor management to pricing strategies. One of its most powerful applications is knowledge transfer. When a manufacturing process is moved to a new facility, AI can synthesize formal work instructions with the captured institutional knowledge of experienced technicians. The result is a comprehensive and unified guide that dramatically speeds ramp-up times while maintaining process integrity.
Engineering for Power and Speed
Integrating AI into embedded systems escalates the demand for higher power densities to support advanced processing chips, which directly conflicts with the industry’s strict requirements for Size, Weight, Power and Cost (SWaP-C). This dynamic creates a critical thermal management challenge, as inefficient power supplies are a primary source of excess heat that can compromise system performance and require costly cooling solutions.
A parallel demand for faster data transmission presents distinct physics-based challenges, as compact systems require smaller connectors that make it harder to maintain signal integrity. The choice of transmission material becomes a strategic decision. While copper remains prevalent for many ruggedized military systems, fiber optics is gaining wider adoption, especially in the satellite market where weight and data throughput are critical. This divergence means there is no single, universal solution. The optimal choice requires a careful balance of performance, weight and environmental considerations.
The Physical Imperative of Ruggedization
Operational environments in aerospace and defense expose components to constant shock, vibration, moisture and contaminants. Adapting established commercial technologies for survival in these conditions remains a significant engineering challenge, often described as a “heavy lift,” that goes far beyond simple protective measures and requires a component-level redesign.
These specialized techniques are critical for building inherent durability. Electrical contacts, for instance, can be screw-machined from solid metal stock instead of stamped from sheet metal, making them far more robust, resilient and resistant to failure from vibration. Another common process is potting, where the backside of a connector is filled with a durable compound. The compound acts like a glue, holding every internal component in place to prevent damage from shock while sealing the unit against moisture and contaminants.
Solutions proven in the automotive sector provide a particularly valuable template for this work. The automotive industry has decades of experience designing connectors for high-vibration and high-amperage applications, such as under-hood and wiring harness systems. This expertise offers a strong starting point for developing the next generation of interconnects for military land systems, including tanks and other tactical vehicles.
The Strategic Shift to Modular Design
The explosive growth of the satellite market is creating an urgent demand for solutions that shorten design cycles and support a diverse range of payloads. In response, the industry is shifting toward standardized, modular and stackable interconnects. This move relies on the adoption of open standards, such as the Modular Open Systems Approach (MOSA) and Sensor Open Systems Architecture (SOSA), which are critical for improving system interoperability and accelerating integration.
The industry is already implementing these standards, with frameworks like SOSA defining standard interfaces for critical functions, such as the payload connection for active optical cables. Designing to a common standard enables manufacturers to create versatile, off-the-shelf systems that reduce development time and facilitate rapid payload integration.
The Geopolitical and Supply Chain Reality
A significant increase in European defense spending is leading US prime contractors to form local joint ventures, creating new mandates for regional production. This trend occurs alongside immense global demand, with a projected 8% compound annual growth rate for the aerospace and defense electronics market through 2030. The combination adds significant pressure to a supply chain already constrained by long lead times for specialized materials and machined components. Consequently, localized manufacturing is becoming a strategic necessity for meeting regional demand and insulating supply chains from geopolitical risk.
This localization strategy also directly addresses complex regional compliance frameworks. Regulations like International Traffic in Arms Regulations (ITAR) and data localization rules, which restrict the sharing of sensitive data across borders, make a regional presence essential for efficient design and production.
From Principle to Practice: Turning Aerospace and Defense Industry Technology Trends into Real-World Systems
The non-negotiable principle of integrity guides every technological and supply chain decision. Putting this principle into practice requires strict adherence to regulatory, security and trade compliance. In an industry with incredibly high stakes, this level of diligence builds durable relationships that are essential for mutual success. A dedication to integrity forms the bedrock of trust, allowing AirBorn, a Molex company, to deliver the reliable, high-performance solutions customers depend on as AI-driven processing requirements and rapid electrification reshape the future of aerospace and defense.
Translating these principles into practice requires a new generation of technologies designed for the industry’s most pressing challenges. The forces driving next-generation systems, including AI and the push for electrification, intensify the pressures of power distribution, thermal management and high-speed connectivity. These demands are met with high-efficiency VPX Power Supplies engineered to manage intense thermal loads and robust Backplane Connectors that prevent signal degradation at high data speeds. Similarly, the strategic shift toward modularity is addressed by standardized solutions, such as FOCuS Active Optical Cables, which offer a pre-qualified interface for satellite payloads. These solutions are complemented by a growing portfolio of ruggedized RF Connectors that satisfy the dual requirements of durability and high-frequency performance in harsh environments.
Explore the solutions powering the future of aerospace and defense.
Additional Resources
Share