The smartphone has changed forever the way we interact with technology. The touch screen technology that we now take for granted would have appeared the stuff of science fiction two decades ago. There is now an entire generation of users who do not remember the conventional rubber keypads of the old cell phone.
As this technology becomes more common, consumers are expecting their other devices to boast the same touch functionality, and manufacturers like Molex have responded with the latest capacitive touch switches
Capacitive touch switches use the same science as the touchscreen of smartphones. They work by using an electrical field that detects objects in proximity to the switch. The switch measures the change in capacitance created by the user’s finger, which in turn causes the switch to actuate.
The capacitive touch switch offers a number of advantages over traditional push-button switches. The functioning of a touch switch does not require physical actuation, which means that there are no moving parts that can wear out. Another advantage can be seen in the adaptability of capacitive touch switches. Unlike its conventional counterpart, a touch switch can be programmed to adapt to circumstances.
The increasing adoption of smart home technology provides an excellent example of the usefulness of touch switches. Smart home control devices can be fitted with capacitive touch switches to control applications as diverse as heating, lighting and security systems. The role of each switch can change according to the system being controlled.