Skip to main content
Image

Antennas

Antenna Solutions

Antennas help enable the wireless connectivity at the heart of today’s high-speed communications—advancing information sharing, delivering seamless in-car entertainment and expanding the Internet of Things. As one of the world’s largest and most trusted antenna innovators, Molex empowers our customers with concept-to-completion solutions for an extensive range of applications including industrial, cellular, 5G, automotive, GNSS/GPS, scientific, medical and more.

External Antennas

Cabled External Antennas offer best-in-class RF performance in ruggedized thermoplastic enclosures that are resistant to moisture, extreme thermal conditions, shock and vibration for convenient mounting in a range of locations

Internal Antennas

Molex leverages its industry-leading expertise and capabilities to design and manufacture custom antenna solutions for a range of wireless and mobile applications, focusing on small multiband and complementary antennas and employing MID/LDS, flex, stamped and ceramic technologies, among others

Combo Antennas

Molex Combo Antennas offer expanded frequency ranges to handle a combination of multiple wireless communication protocols, while also delivering long-range connectivity, high-power efficiency, a compact form factor and easy integration

Learn More

Molex’s antenna products are developed with industry-leading RF expertise to ensure best possible connectivity. Molex specializes its Custom OEM Antennas to exactly fit customers’ needs by offering a wide variety of single and multi-band antennas. To fulfill the growing requirements of connected vehicles, Molex developed Smart Antenna Solutions.

Learn More
Image

Molex Electronic Solutions Molex Antenna Solutions


1.  Protocols and frequencies

Wireless protocols and operating frequencies Antennas are defined by the protocol they function for, examples include Bluetooth/Wi-Fi, GNSS, cellular network, ultra-wideband, ISM and NFC. The various protocols correspond to different operating frequencies. For example, Bluetooth antennas operate within a frequency range of 2.4 to 2.485GHz, while NFC antennas operate under a frequency of 13.56MHz. Even within

the same protocol, various frequency bands are allocated. To select the most suitable antenna, users must define both the protocol and operating frequency.

2. Types

Antennas come in different forms and shapes, and what is ultimately selected depends on a consideration

of customer preferences and usage environments. Based on their materials and processes, they can be categorized as a PCB, SMT, FPC, ceramic and external rod antenna. For example, to solder an antenna to the PCB, a surface mount antenna is most appropriate. FPC or PCB antennas can be options when the antenna

is to be placed on the interior wall of the housing and the connection is through an RF connector, while an external rod antenna is likely when the antenna is to be placed on the outside of the product. But because an antenna’s transmission capabilities are very sensitive to its surrounding environment, for optimal results, it is best to determine its position before selecting the type.

3. Sizes

An antenna is designed according to the needed wavelength/frequency of operation. Antennas with sufficient wavelength will perform better than antennas with sub-optimal wavelength. For the best wireless performance, users should choose a bigger antenna if the size of the product permits.

4. Balance

An in-balance antenna is smaller in size, but it uses the PCB grounding as part of the antenna system, whereas a balanced antenna can function by itself although it is bigger. If the size of the product permits, it is better to choose a balanced antenna. If this is not possible, choose an appropriately sized PCB grounding.

5. Performance indicators

The performance of an antenna depends on several indicators, such as impedance, efficiency, S11/VSWR, radiation pattern, gain, polarization and axial ratio.

a. Impedance

An antenna’s impedance needs to align with the output impedance of the wireless module, which is generally 50 Ohms.

b. Efficiency

Antenna efficiency is a key indicator that determines the emissivity of an antenna.It specifies how much energy will be lost during the energy exchange. The greater the efficiency, the better the antenna is. Generally, a value greater than 40% indicates acceptable performance.

c. Return loss (S11) and voltage standing wave ratio (VSWR)

S11 or VSWR indicates the amount of energy reflected in the RF circuit and transmitted to the antenna. The smaller the value, the better it is. Generally, S11≤-6dB or VSWR≤3 would indicate acceptable performance.

d. Radiation pattern.

An antenna’s radiation pattern shows how the antenna radiates in a 3D plane. The radiation pattern depends on the type of antenna and the surrounding environment. If the radiation pattern is tested under a scenario with free space (no surrounding interference), it might not represent the real situational pattern as It will change per environment due to reflections and loading. The pattern will show where and how the gain (described below) is distributed in the 3D space, indicating the strong and weak angles.

Depending on the application, a user needs to select an antenna with an omni-directional or a single directional pattern. Omni-directional antennas tend to be better for general purposes, while a directional antenna would be better for GPS or similar applications.

e. Gain (average and peak).

Antenna gain can be deemed as average gain or peak gain. The average gain is the average of the gain at a frequency across all the angles in the 3D space while the peak gain is the maximum gain at that frequency. The average gain is equivalent to the efficiency and the higher the better. A rounded antenna radiation pattern will have lower peak gain compared to a directional antenna. As with respect to radiation patterns, peak gain will be different in free space and when mounted on the device.

f. Axial ratio

Axial ratio is an important performance indicator for a circularly polarized antenna and represents its purity. Generally, an axial ratio smaller than 3dB indicates good performance.

6. Matching networks

The matching network is designed to optimize the antenna impedance to match 50 Ohms. For an acceptable S11/VSWR of the antenna, some antennas will be required to have a matching circuit. This is normally specified in the application guide. The application guide also references many other guides to achieve optimized antenna performance.

Once the above procedures are completed, the requirements for the antenna become clear. Such requirements are summarized per Table 1 below. The table can then be used to search for an antenna from

the product library of an antenna manufacturer. The Molex antennas are shown in Table 2.

Table 1

No.ItemSpecifications
1Frequency Range2.4 - 2.485 GHz
2TypeFPC
3Antenna Size<40*20mm
4Average Efficiency>50%
5Return Loss<-6db
6V.S.W.R.<3.0
7Peak Gain (Max)>2.0dBi
8PolarizationLinear
9Impedance (Ohms)50

Table 2

DescriptionEquipmentRequirement
Frequency RangeVNA E5071C2.4-2.5GHz5.15-5.85GHz
Return LossVNA E5071C< -10dB
Peak Gain (Max)OTA Chamber2.8dBi3.7dBi
Avg. Total EfficiencyOTA Chamber>70%>70%
PolarizationOTA ChamberLinear
Input ImpedanceVNA E5071C50 Ohms