Skip to main content
Two engineers review information on a laptop while standing among rows of server racks in a data center.

Beyond the Front Panel: 224G Near-ASIC Design for XPO

The XPO Multi-Source Agreement standardizes the pluggable interface for next-generation AI data centers, shifting the competitive battleground to the internal electrical channel. System architects now face the complex task of routing thousands of 224G lanes from the switch ASIC to the front panel without compromising signal integrity or exceeding thermal limits.

Read Time: 5 Min

The eXtra-dense Pluggable Optics (XPO) Multi-Source Agreement (MSA) establishes a common pluggable architecture capable of unprecedented density, condensing 64 channels into an incredibly tight footprint to support 12.8Tbps per module. For context, traditional OSFP architectures require four times the space of XPO. That means an equivalent-bandwidth switch requires 75% less rack space when utilizing the 1OU XPO form factor. Because the MSA standardizes the front-panel interface across the industry, switch vendors can no longer rely on external ports to gain a competitive edge in the hyperscale market.

As a result, the true differentiator for AI switch performance now lies in the electrical channel connecting the ASIC to the front I/O. Treating 224G near-ASIC design for XPO as an afterthought can lead to severe signal degradation and thermal failures at these speeds. The transition to XPO is a major evolutionary jump in copper signaling, prompting a new way of thinking about how data travels through the last few inches of the switch.

The Physical Realities of the XPO Electrical Channel

Routing hundreds of high-speed differential pairs across traditional PCBs to feed front-panel XPO modules can result in significant signal loss and thermal bottlenecks. To make these architectures viable, system designers need to address three distinct physical challenges.

The Radix and Density Problem
AI training clusters demand an ultra-high switch radix to minimize the number of network layers and efficiently connect tens of thousands of GPUs. While XPO solves density at the front panel, it creates extreme routing congestion at the center of the board.

To support the massive throughput of these front-panel modules, hundreds of 224Gbps PAM-4 differential pairs must exit the switch ASIC simultaneously within a highly constrained 1OU space. The physical real estate around the ASIC is at an absolute premium, making it incredibly difficult to fit the necessary physical gates and terminations. Complicating matters, the 224Gbps PAM-4 modulation scheme leaves very little signal margin, meaning any physical imperfection in the channel drastically impacts data transmission.

The Limits of PCB Routing
The PCB acts as a physical barrier, draining signal strength and closing the signal eye diagram before the data ever reaches the XPO front-panel ports. In fact, high-performance PCB traces can lose 0.5 to 1 dB per inch of travel. Pushing high-frequency signals through solid PCB material consumes significantly more power than routing through twinax flyover cables. As a result, that energy loss converts directly into heat, eventually exceeding the thermal carrying capacity of traditional air cooling.

Tightening Thermal Constraints
With XPO, primary cooling takes place within the transceiver module. This leaves the host side, which is densely packed with high-speed cabling and power delivery components, to operate in higher ambient temperatures. In this environment, every physical transition in the signal path introduces potential impedance mismatches and further thermal strain on the system. Consequently, balancing signal integrity with thermal responsiveness becomes the central engineering hurdle for the internal switch architecture.

Navigating 224G Near-ASIC Design for XPO from the ASIC Outward

A successful XPO implementation begins at the ASIC. To bypass the PCB and reach the front panel via high-speed flyover cables, architects must first choose between near-ASIC and on-substrate connectivity.

Bypassing the Board
High-speed twinax cables act as a bridge over the lossy PCB material, flying the signal directly from the ASIC landing spot to the XPO interconnect. At 224G speeds, this flyover method is the mandatory pathway for modern system design.

Routing signals through cables rather than board traces preserves electrical margins and reduces overall power consumption. During this process, engineers weigh the trade-offs between signal integrity and physical routability, deciding whether to bend cables to fit tight spaces or keep them straight to minimize loss.

The Near-ASIC Approach
Landing the connection just outside the chip package offers a mature, highly adaptable routing strategy to support the dense front-plate radix of XPO switches. Customers prioritizing rapid deployment and simplified manufacturing often opt for 224G near-ASIC design for XPO to avoid disrupting the delicate silicon substrate. In these scenarios, adjusting the connection pitch gives designers flexibility when board real estate dictates a slightly wider footprint.

The On-Substrate Approach
Alternatively, connecting directly to the ASIC package delivers the most direct electrical channel and minimizes crosstalk. System designers approach the chip package as highly restricted territory, only breaking into that space when electrical performance targets make off-substrate routing impossible. Moving onto the substrate introduces a highly complex environment. Engineers must integrate physical connections directly into third-party silicon packaging that was not originally designed to support them. Architects choose the on-substrate route when pushing the absolute limits of channel performance or preparing for future bandwidth jumps.

System-Level Optimization for Next-Generation AI

Scaling these architectures for future generations hinges on considering the entire signal path as a single, cohesive ecosystem.

The Danger of Fragmented Design
Sourcing individual connectors, cables and cages from different vendors introduces severe interoperability risks and unpredictable performance drops. This fragmented approach often fails to account for how thermal dynamics and signal integrity interact across the complete channel. Without a fully integrated solution, both mechanical and electrical engineering teams face never-ending challenges in their march toward a production-ready design due to the strict 1OU constraints of the XPO MSA.

Designing for the Future
The XPO MSA already outlines a pathway to 448G, making current architectural decisions critical for long-term scalability. With this progression in mind, system designers weigh physical cable routing against signal loss to build a physical layer capable of handling faster modulation schemes down the road. Ultimately, preparing for future AI architectures means selecting internal connectivity that supports higher bandwidth densities without forcing a complete chassis redesign.

Engineering the Complete XPO System Implementation

Leading with a single technology forces customers into unnecessary design compromises and limits their ability to scale. To solve this, Molex combines comprehensive engineering experience with a diverse technology portfolio to build reliable XPO architectures from the chip to the front panel. This full spectrum of options allows architects to build the right end-to-end architecture for their specific needs.

For customers prioritizing the fastest time to market, lowest implementation risk and familiar PCB manufacturing, Molex offers CX2 near-ASIC connectors. For designs where minimizing insertion loss and crosstalk is critical, the Impress Co-Packaged Copper Solution features a reworkable, compression-based socket that protects the substrate and provides flexibility during assembly.

Whether connecting near the ASIC or directly on the substrate, BiPass cable assemblies and specialized cage designs complete the channel, successfully fitting the high density of XPO modules within standard 1OU height constraints.

By owning the complete electrical channel, Molex guides customers toward the ideal system architecture for their specific performance targets. Discover how Molex near-ASIC connectivity solutions optimize the full signal path to make next-generation XPO architectures possible. 

Additional Resources


Application

Next-Generation Near-ASIC Connectivity

At 224G and beyond, bandwidth, power and density constraints require addressing electrical, mechanical and thermal factors early in system design. Molex combines high-speed connectivity expertise with collaborative engineering support to optimize the full signal path for demanding near-ASIC architectures.

Application

Co-Packaged Copper for AI Data Centers

At higher bandwidths, long board-routed copper paths introduce signal loss that can limit channel performance and increase power demands. Molex co-packaged copper solutions bring high-speed connectivity closer to the ASIC to shorten channel length, reduce power draw and support next-generation data center architectures.

Close-up of a server-grade CPU socket architecture, demonstrating the high-density pin layout required for co-packaged copper interconnects.

Product

Impress Co-Packaged Copper Solution

At 224G speeds, PCB trace loss can compromise signal integrity, while soldering directly to the ASIC risks damaging expensive silicon. The Molex Impress Co-Packaged Copper Solution uses a compression socket to connect directly to the ASIC substrate without drilling or soldering, enabling a lower-loss, more serviceable high-speed channel.

Molex Impress Co-Packaged Copper Solution mounted to a PCB.

Share