Read Time: 7 Min
Electromagnetic interference (EMI) is a constant battle in aerospace and defense applications. As systems grow more advanced, interference becomes harder to predict and control. High-speed digital and RF components now operate at extreme frequencies, where even minor levels of EMI can cripple radar, compromise encrypted communications or throw avionics off course. Without effective filtering, signals degrade, operations falter and mission success may be put at risk.
Left unchecked, EMI threatens security and erodes performance. Every system in a military aircraft—from flight controls to targeting—must block (or attenuate) interference before it reaches sensitive electronics. Engineers designing for high-noise environments cannot afford last-minute fixes that introduce risk. As frequencies climb and system complexity grows, engineers must find ways to keep interference from derailing a mission.
EMI Filtering Techniques in Aerospace and Defense Components
Effective EMI management goes beyond blocking noise. It requires careful engineering to balance cut-off frequency, insertion loss and other design constraints at pivotal entry points.
Pi filters, using a three-element configuration (capacitor-inductor-capacitor), absorb high-frequency noise in power and signal lines. Their sharp attenuation slope makes them ideal for broadband EMI suppression, particularly in power supply lines where voltage fluctuations and switching noise create disruptive harmonics.
Feedthrough capacitors inhibit unwanted signal transfer at interconnect points by providing a low-impedance path to ground. They effectively reduce conducted emissions, especially in shielded enclosures where traditional capacitors fall short.
Inductive elements (e.g., ferrites, toroids) absorb high-frequency energy and dissipate it as heat, minimizing unintended coupling. Their effectiveness depends on impedance characteristics, material composition and frequency range, making them vital features in high-speed data and power applications.
Shielding and grounding techniques keep emissions contained and block external interference. Properly designed shielding reduces radiated emissions and noise and works alongside filtering components to control both conducted and radiated EMI.
Validating EMI Performance
In aerospace and defense, EMI filtering is more than a design consideration—it is a requirement. Their systems must meet MIL-STD-461G, the industry benchmark for electromagnetic compatibility (EMC), establishing strict testing to confirm that electronics limit emissions and resist external interference. Two key tests—RE-102 and RS-103—serve as dual safeguards against EMI threats.
RE-102 (Radiated Emissions) measures unintended electromagnetic radiation to prevent interference with mission-critical electronics. Spanning frequencies from 10 kHz to 18 GHz, this test confirms that avionics, secure communications and radar systems operate without disrupting each other. Naval systems are held to even stricter limits (2 μV/m or lower) to ward off sonar interference.
RS-103 (Radiated Susceptibility) subjects components to high RF exposure, verifying that they function reliably under extreme electromagnetic fields. Frequencies extend up to 40 GHz, simulating real-world threats such as radar-guided missile seekers, electronic warfare jamming and high-powered transmissions. Components that fail under these conditions are unacceptable solutions for military or aerospace applications.
MIL-STD 220 (Military Standard) evaluates the resilience of electronic components against harsh environmental and mechanical conditions. This standard tests for factors like thermal shock and vibration—both crucial for aerospace and defense systems where extreme temperatures and constant motion can degrade performance. Components that fail these tests risk operational failure in high-stress environments, making compliance essential for mission-critical applications.
Meeting these rigorous standards helps ensure EMI-filtered components are reliable, enabling aerospace and defense systems to operate in real-world scenarios.
EMI Protection Beyond Aerospace
Outside of aerospace and defense, industries such as healthcare and industrial automation, along with sectors supporting critical infrastructure—including power grids, transportation systems and emergency networks—also face EMI risks.
In medical technology, interference-free operation can truly mean the difference between life and death. Momentary EMI bursts could destabilize life-support systems in operating rooms, putting patients at risk. The same filtering technology that protects avionics and secures military communications also keeps medical devices stable.
Industrial automation faces a different concern: unpredictability. EMI does not always cause outright failures, but it may cause intermittent errors that are notoriously difficult to diagnose. Good filtering avoids costly downtime in robotic systems, automated production lines and sensor networks that depend on steady signals.
Power grids, transportation systems and emergency networks use EMI filtering to fend off outages and communication errors. A single EMI-related failure in these systems can have massive consequences, making interference mitigation vital to ensuring the proper functioning and performance of public infrastructure.
As more connected devices come online, EMI threats escalate. Filtering is about more than eliminating interference—it is about keeping essential systems functional in an increasingly congested spectrum.
Expanding EMI Filtering for Critical Applications
To meet growing aerospace and defense demands, Molex has broadened its EMI-filtered interconnect and RF component lineup. These additions strengthen our ability to support core systems. The latest EMI-filtered D-sub adapters and connectors provide electromagnetic shielding and filtering at primary system entry points, preventing unwanted noise from reaching sensitive electronics. New EMI filter plates, fixed RF coaxial attenuators and RF coaxial terminations enhance signal stability, regulate power and minimize disruptions.
With more than 250 configurations and extensive customization options, these solutions align with both commercial and application-specific designs. With this expansion, Molex is strengthening its role in aerospace and defense, accommodating industry demand for more reliable and integrated systems.
Key Differentiators of Molex EMI-Filtered Interconnects and RF Components
D-Sub Adapters and Connectors
Molex EMI-filtered D-sub adapters and connectors suppress electromagnetic noise at system entry points, protecting sensitive electronics. A one-piece die-cast shell and fully soldered internal structure reinforce both mechanical and electrical performance and prevent failures in high-vibration environments. M24308-compatible standard and high-density options fit seamlessly without cable or PCB modifications.
EMI Filter Plates
Filter plates block interference at enclosure boundaries, preventing electromagnetic noise from compromising system reliability. Replacing discrete filtering components, they conserve chassis and PCB space while maintaining signal clarity. Configurations with up to 50 filtered lines adapt to different enclosure sizes and materials.
Fixed RF Coaxial Attenuators
Attenuators regulate signal strength to avoid overload in high-frequency applications like radar and secure communications. Designed to handle up to 100W, they provide consistent attenuation across application-specific frequency bands and are compatible with MIL-STD-348 RF connectors.
RF Coaxial Terminations
Terminations absorb excess RF energy, eliminating reflections that distort signals. Engineered for aerospace and military applications, they stabilize impedance and enhance signal integrity. Solderless contact construction reinforces stability under vibration, shock and temperature extremes.
Military-Grade Durability and Compliance
Each component meets MIL-STD-202 standards for thermal shock, vibration and mechanical shock. Ruggedized construction ensures dependability in environments where interference and mechanical stress threaten stability.
By incorporating EMI-filtered interconnects, filter plates, attenuators and terminations, Molex solutions minimize interference across mission-critical systems. Engineers now have a broader selection of components designed to integrate smoothly while delivering strong EMI resistance under electromagnetic stress.
Molex: Committed to EMI Protection in Aerospace and Defense
EMI challenges are not going away. As aerospace and defense systems push toward higher frequencies and greater integration, filtering solutions must adapt alongside them. Molex strengthens interference mitigation by leveraging dedicated in-house capacitor manufacturing with advanced shielding and mechanical reinforcement, delivering continuous performance even under extreme environmental and electrical stress.
Defending devices from EMI should not be an afterthought—it is imperative for preserving reliable operation in aerospace and defense. As electronic systems grow more complex, interference control must keep pace to maintain uninterrupted operation in environments where failure is not an option. Explore Molex EMI-filtered interconnects and RF components tailored for vital aerospace and defense applications.
Share